Design Summary Tool

The Design Summary tool enables users to perform an intelligent search of information contained within Compatible Units (CU) and Work Locations (WL) of designs. Clicking the tool launches a dialog, the Design Summary form, that mimics the design tree and provides information about the design and the CUs. The Design Information and Compatible Units groups can be expanded to show more information, including details about all the CUs in the design.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?