Edit Graphic Favorite Name

Once a graphic favorite has been created, only its name may be edited. To modify the name of an existing graphic favorite, you must have an edit session started.

  1. Begin an edit session. If you do not have an edit session started, the right-click utility that allows you to edit a graphic name will not be available.
  2. Right-click the graphic favorite and select Edit Graphic Favorite Name.

  3. Type a new name for the graphic favorite and click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?