Graphics Tab

The Graphics list allows you to create and store graphic elements for placement on the map. Graphic favorites may be placed without an edit session started. To create graphic favorites or categories, you must begin an edit session.

To view the Graphics list, click the Graphics button  on top of the Table of Contents.

The Active Annotation Target tool provides the flexibility to place graphics in two different formats: graphic and annotation.

 

Graphics list in ArcFM Desktop applications (ArcFM, Designer, or ArcFM Viewer AND the Redliner extension).

You can rearrange the list of graphic groups. Drag and drop groups within the gray part of the list (not in the white space below).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?