Placing a Template Favorite - Select CU
Designer prompts the user to select a compatible unit (CU) when the user places the template favorite with a design open. The program adds all features the user places on the map with the template favorite to the open design.
- Instructions from your administrator will appear in the white bar at the top of the dialog ("Select a compatible unit." in the example above).
- Unselect the Apply to Remainder checkbox to choose a CU for each feature in the series. Leaving this checkbox selected applies your selection to all features in the series. If this checkbox is disabled, the feature isn't part of a series or is the last feature in a series.
- Select a CU in the Compatible Unit(s) field. If a CU appears
under the GU node in the Feature(s) window, Designer will use this
CU as a default. Select a CU and click OK. There are three buttons
to help you easily find the appropriate CU: Find Next, Delete, and
Browse.
The Find Next button performs a search. Type the first few letters of the CU in the field. Click this button to search for matching CUs. Hit the Enter key to select the found CU and add it to the window at the left.
The Delete button clears the contents of the field.
Like Find Next, the Browse button performs a search. Click this button for a window to search for a CU. You can also select a different work function on this screen if another is available.
- You can use the Add Non-GIS CUs button to add a non-GIS CU.
- Click Next > to continue placing the template favorite.
- You can click Finish to complete placement of the template favorite, accepting as many defaults as possible. You will still be prompted for any required actions.