Designer Toolbar
The Designer toolbar accesses a collection of tools that increases productivity and functionality during ArcMap sessions. If the Designer toolbar is not displayed, click View > Toolbars, then check Designer on the dropdown list. Or you can right-click in the gray toolbar area and select Designer from the list. This toolbar is dockable.
: Designer
CU to WL Assignment
The following button does not appear on the toolbar by default and must be added using Tools > Customize.
- To add buttons to the toolbar:
- Right-click the gray area of the toolbar and select Customize.
- Select the Commands tab and click ArcFM Solution.
- Drag icons from Commands and drop on the toolbar.
- To remove buttons from the toolbar:
- Right-click the gray area of the toolbar and select Customize.
- Drag the button from the toolbar and drop it anywhere off the toolbar.
- To restore default buttons:
- Click the Toolbars tab.
- Highlight the toolbar you want to reset.
- Click Reset to restore any removed default buttons.