ArcFM Underground Facility Diagrams Toolbar
This toolbar provides the tools to create new underground facility diagrams as well as view and edit existing diagrams.
![]() |
Launch Diagram Manager |
Use this tool to either create a new diagram or view an existing one. You must have an editing session started to create a new underground facility diagram. This button will be disabled if the following layers are missing from the map: Floor, Wall, Duct Bank, Duct. |
![]() |
Close Diagram Manager |
Click this button to dismiss the Diagram Manager window. |
![]() |
Navigate to Next Facility |
Click this button, then click a conduit or duct bank to navigate to the next underground facility. |
![]() |
Navigate to Previous Facility |
Click this button to navigate to the previous underground facility. This button will remain disabled until the Navigate to Next Facility button has been used. |
![]() |
Select Diagram |
Click this button to select the current underground facility diagram. This is necessary when using the Save As Favorite tool. |
![]() |
Select Duct Bank |
Click this button, then click a duct bank to select it. This is necessary when using the Save As Favorite tool. Use the Shift key to select multiple duct banks. |
![]() |
This tool allows you to create a map grid that encompasses the underground structure as well as your underground facility diagram. To enable this tool, you must have selected an underground structure that has a facility diagram created. |