Flip Duct Bank View in Diagram Manager
You can reverse the view of a duct bank diagram to match the numbering of its opposite pair. For example, in the following image, notice both duct diagrams in the connected manholes use the same numbering configuration. In fact, this is incorrect, as one manhole should have the opposite numbering configuration to reflect the true installation in the field:
After using the flip tool, notice the duct diagram in MH201 is flipped to show the opposite numbering configuration of MH200:
To flip the duct bank view, follow these steps:
- Using the Launch Underground Facility Manager
tool,
click the underground structure where you need to flip the duct bank
diagram. - In the Diagram Manager, click Edit Duct Bank.
- Toward the bottom of Diagram Manager, click the Select Duct Bank to Flip tool.
- Bring your cursor into the map, then click the duct bank that needs to be flipped (the duct bank highlights in green in response to your cursor).
- Confirm the numbering has been flipped, and Save your edits.