Getting Started with Fiber Builder

Fiber Builder is found on the Main Menu > Fiber tab.

When using Fiber Builder for the first time, keep the following in mind:

  • If you are a Fiber Admin, you do not need to be in a Session in order to create and manage fiber favorites. However, you do need to be in Edit Mode within ArcGIS Pro.

  • If you are a Fiber Editor, edit work is for fiber locations and favorites is done within a Session.

    Everybody in your company sees the same set of fiber favorites. All fiber favorites are available to Fiber Editors regardless of what session they are in.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?