Modify Attributes or Delete an Existing Circuit

To modify the attributes of an existing circuit, follow these steps:

  1. Locate the circuit as described above.

  2. Double-click the circuit name to populate the Fiber Circuit Details pane.

  3. Update the attributes as needed.

  4. Click Apply.

  5. To delete a circuit, follow the steps above, but once your circuit is within the Fiber Circuit Details pane, click Delete Circuit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.