Open Fiber Connections

Whether viewing or editing connections, the procedure to open a fiber point feature in Fiber Connections is the same. The Fiber Connections tool only interacts with point fiber features.

To open a fiber point feature to view its connections, follow these steps:

  1. On the Main Menu > Fiber tab, click Fiber Connections.

  2. Click a fiber point feature in the map. The Fiber Connections pane opens and shows the last place you positioned it.

    The corresponding highlighted cables are also seen on the map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.