Disconnect

You can disconnect existing connections in Fiber Connections.

  1. Create a Session or opening an existing Session.

  2. On the Main Menu > Fiber tab, click Fiber Connections.

  3. In the map, click the fiber point feature that requires fiber connection work.

  4. In the window that opens, use the connection menus to find the fiber assets that need disconnecting.

  5. Click the connection that needs updating once. Or, use Shift and Ctrl to choose multiple connections. Chosen connections are highlighted in blue.

  6. Press the Delete key. Notice the connections disappear.

    There is no Undo button in Fiber Connections. Click Cancel to roll back any edits prior to the last time you clicked Apply.

  7. Click Apply and save your session.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.