Export and Import Favorites

After creating favorites, you can export them to a JSON file. This is a way to create backups of favorites or to transfer them to other environments.

  1. In Fiber Builder > Favorites, right-click the favorites folder and choose Export folder:

  2. Alternatively, right-click the favorite itself and choose Export favorite:

  3. Click Save.


After performing an Export of your favorites, you can import them into a different environment.

  1. To Import, locate the exported JSON file then drag and drop it into Fiber Builder > Favorites.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.