Edit Existing Fiber Locations

The Fiber Builder pane allows you to edit “the inside” of existing fiber facilities. You can delete parts of fiber facilities or drag and drop Favorites into existing fiber facilities. For example, you can drag and drop a rack and patch panels from the Favorites into an existing patch location.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.