Getting Started

Welcome to Fiber Manager XI. Here are helpful links and other notes to get you started.


Links


Important Notes Before you Start Working in the Map

  • In ArcGIS Pro, do not change the names of the layers in the Contents pane, as the toolset is using those names to provide relevant functionality. If you need to change the names, work with your administrator to ensure the names are the same across the map, Solution Center, and the ArcGIS Portal.

  • Your Fiber Manager XI login must be the same as the login you use for Session Manager. Mixing logins produces errors when you attempt to save your work. For more information about Sessions, see the Session Manager help topic.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.