NHA2778902-12

Data recording (PM2230)

The meter stores each new minimum and new maximum value with date and timestamp for all instantaneous values (average, total, and each phase).

The meter also records the following:

  • Alarms (with 1s timestamping)

  • Parameters configured for data logging

  • Data, alarm history, and diagnostics logs

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?