EcoStruxure Power CommissionLogiciel
Présentation
EcoStruxureTM Power Commission est le nouveau nom du logiciel Ecoreach.
EcoStruxure Power Commission software helps you to manage a project as part of testing, commissioning, and maintenance phases of the project life cycle. The innovative features in it provide simple ways to configure, test, and commission the smart electrical devices.
EcoStruxure Power Commission software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.
Le logiciel EcoStruxure Power Commission permet de configurer les disjoncteurs, modules et accessoires suivants :
|
Gammes de disjoncteurs |
Modules |
Accessoires |
|---|---|---|
|
Disjoncteurs MasterPact MTZ |
|
Module de sortie M2C |
|
|
Modules de sortie M2C et M6C |
|
|
Modules de sortie SDTAM et SDx |
|
(1) Pour l'afficheur FDM121, le logiciel permet seulement de télécharger le firmware et les informations de langue. |
||
Pour plus d'informations, consultez l'aide en ligne d'EcoStruxure Power Commission.
Le logiciel EcoStruxure Power Commission est disponible à l'adresse www.se.com
Fonctionnalités clés
EcoStruxure Power Commission software performs the following actions for the supported devices and modules:
-
Create projects by device discovery
-
Save the project in the EcoStruxure Power Commission cloud for reference
-
Upload settings to the device and download settings from the device
-
Compare the settings between the project and the device
-
Perform control actions in a secured way
-
Generate and print the device settings report
-
Perform a communication wiring test on the entire project and generate and print test report
-
View the communication architecture between the devices in a graphical representation
-
View the measurements, logs, and maintenance information
-
Export Waveform Capture on Trip Event (WFC)
-
View the status of device and IO module
-
View the alarm details
-
Buy, install, remove, or retrieve the Digital Modules
-
Check the system firmware compatibility status
-
Update to the latest device firmware
-
Perform force trip and automatic trip curve tests