2505_LSS100400_SW_04.0

Device Actions

There are seven icons at the end of each device line. When you click these icons, you can do the following:

  • Upgrade device firmware

  • Allow joining through this device

  • Identify device

  • View device information

  • Set device control and status

  • Set device parameters

  • Configure the device

  • Delete device


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?