2505_LSS100400_SW_04.0

Network Map

The Network map function graphically displays the mesh network topology with color-coded links between individual devices. Each link means communication between the devices (sending telegram).

You can filter links by clicking on the menu on the top left:

  • Child

    : The device that reaches controller through another device (through parent device).
  • Parent

    : The root device that other devices connect to as a children.
  • Sibling

    : A device that the other device can “hear”, but is not connected to it.

    Active route: Active connection.

The percentage means the strength of the mesh network signal (this data comes from the router).

Make sure all devices have enough signal to be controllable. Signal strength is also displayed during monitoring – see Monitor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?