2505_LSS100400_SW_04.0

Add Install Code

The Add install code function enables encrypted commissioning of your devices. It is the secure way how to commission your devices. You do not share the network information, for example, the network key.

You need to find out the following information from the QR code of your device:

  • Address (EUI-64): MAC address

  • Install code

To enable encrypted commissioning of your device, follow these steps:

  1. Click > select Add install code.

  2. Enter the MAC address and install code of your device > click Add.

NOTE: If your controller disconnects or reboots while adding the installation code and MAC address, you have to start over.

Now commission your device as described in Pairing the Device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?