2505_LSS100400_SW_04.0

Hybrid Module Firmware Upgrade

The firmware is distributed as part of the Hybrid plugin. Once you have connected the Hybrid Module to your controller and downloaded the Hybrid plugin, a firmware update is automatically triggered to bring new features (new devices, new functionalities) and security patches.

The Module firmware version number displays in the Configuration section in the lower left corner of the screen (Configuration). If you are connected via VPN, this information is not visible.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?