2505_LSS100400_SW_04.0

Pairing the Device

If your wireless device is battery powered, make sure you have a battery inside and remove the plastic film from the battery. If the device is mains powered, make sure it is properly connected to the mains.

Find the Reset/Setup button on the back of your device. With this button, you can pair your device and reset it.

NOTE: If your ZigBee device does not have this button, follow the instructions in the device user manual.

You can also commission the devices using the Schneider Electric eConfigure software tool (see more here https://www.se.com/ww/en/download/document/eConfigure_ETS5_Lite175/).


You have to open your network to add the ZigBee wireless devices.

  1. Click the Network state button at the top right. The change network state dialog appears:

  2. Click Yes to change the network status to Open.

  3. Set your device to pairing mode (see Device Pairing Mode).

    NOTE:

    Your commissioned wireless device flashes orange after a triple-click. If the network is open, your device flashes green for a few seconds, and a new device line appears in the plugin. Your device is paired.
    Address: Short and long address of the device
    Manufacturer/Model: Device identification
    Status: The time last telegram was sent

    IMPORTANT: It is recommended to check pairing procedure of your ZigBee device in the user guide of the device. The pairing process may vary between the devices.

  4. If you are not adding any more devices, close the network. Click the Network state button at the top right again and click Yes to change the network status to Closed.

NOTE: The network closes automatically 10 minutes after opening. You can extend this interval. See more in Configuration.

NOTE: The green background of the status column means that data is being sent or updated.


Incomplete commissioning of battery devices

If you see question marks in the Manufacturer/Model column in the device line after commissioning, the device is not correctly commissioned, even if it looks like it.


Such a device would not work properly. If this happens, delete the device from the device list and configure it again. It is possible that you will need to commission your device repeatedly.

Do not forget to wake your device before deleting.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?