2505_LSS100400_SW_04.0

Identify Device

The Identify device function is used to identify a device on the network.

When you click , the device will start blinking or lighting up for about 15 seconds to identify itself.

This feature is useful when you are unsure which device is which.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?