2505_LSS100400_SW_04.0

Setting Device Parameters

With , you can change the device parameters. The function is disabled for devices that do not have configurable parameters ( appears light gray = inactive).

Opening the Parameters dialog:

  • Click on the Parameters icon: .

  • A dialog box will open where you can set individual values depending on the type of device.

Troubleshooting:

  • If the device does not respond (Parameters dialog box does not open):
    1. Check if the device is turned on.

    2. Try waking it up by interacting with it.

    3. If that does not work, press the device's programming button and immediately click Continue.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?