2505_LSS100400_SW_04.0

Launching the Start Page

The following procedure is the same for both new and existing installations. After successful login, the next step gets you to the start page.

NOTE: It is recommended that you have the latest firmware in your controller.

Install the Hybrid plugin to configure your wireless devices:

  1. Click in the upper right corner.

  2. A list of available applications that you can install will open.

  3. Find the Hybrid plugin and click the download icon at the end of the line.

  4. Click Yes to install the plugin.

You can also install the plugin from a file on your computer (for example, if your controller does not have an Internet connection).

The Hybrid plugin will appear in your list of installed items.

When you return to the start page, you will see that the Hybrid plugin icon appears among your available applications as KNX Hybrid:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?