2505_LSS100400_SW_04.0

Allow Joining through This Device

This function allows you to initiate the pairing process through a specific device. For example, you can pair a sensor through a nearby socket. New devices can join the network but only through the selected router.

Steps to pair devices

  1. Open the pairing dialog:

    • Click .

    • A dialog box will appear asking if you want to change the network status to Open.

    • Click Yes.

  2. Pair the device:

    • Follow the instructions in the Pairing the Device chapter to complete the pairing process.

  3. Close the network:

    • Once pairing is complete, click the Network state: open button at the top right.

    • Click Yes to close the network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?