2505_LSS100400_SW_04.0

Preparing Your Module for Pairing

After you install the Hybrid plugin on the controller, you can pair your wireless devices to your controller. You can change parameters and group objects for each device.

  1. Open your browser and connect to your controller.

  2. Click the KNX Hybrid icon on the start page. This will take you to the plugin start page, which displays a list of the wireless devices.

KNX Hybrid icon on the start page

If you have not added any wireless devices yet, the list is empty.

Plugin home page

Make sure the Hybrid Module functionality indicator in the upper right of the home page is green (). If the indicator is red, or if the Network state button next to it is missing, the Hybrid Module is not working properly and you need to reboot your controller.

NOTE: If you are accessing the module remotely via VPN, the indicator flashes red, and the Network state button is missing, even if the module is working. You cannot open and close the network remotely.


If there is no communication and the installation does not work, follow these steps:

Reboot your controller:

  1. Close the Hybrid plugin with the cross at the top right.

  2. On the Start page, click on the ConfiguratorSystemSystem tab.

  3. Select Reboot from the menu.


After you reboot your controller:

  1. Return to the start page.

  2. Prepare your wireless device that you want to pair.


NOTE: If a reboot does not help, try to power your device off and then on.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?