2505_LSS100400_SW_04.0

Workflow

This overview shows the sequence of the entire process of commissioning the Hybrid Module up to visualization and integration with the Wiser KNX application.


*If the ZigBee device starts updating its firmware, it closes the network, and other ZigBee devices do not appear in the list of discovered ZigBee devices.

The firmware update process can take up to 20 minutes.

After the firmware update is complete, open the network again and continue pairing the other ZigBee devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?