2505_LSS100400_SW_04.0

Create New Object

To create a new object:

  1. Click at the end of the device line.

  2. Click above the object drop-down menu.
    A dialog will appear in which you can select the type of object.


    Types of objects

    • Standard object – object value changes are sent to the KNX bus.

    • Virtual object – object value changes are never sent to the KNX bus.


      (Virtual objects are usually used for visualization or scripting.)

  3. In the Create object dialog, click Create standard/virtual object.

  4. Fill in the Add new group address form > click Save.

The new object appears in the object field of the Configuration form. Click Save to save the changes.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?