2505_LSS100400_SW_04.0

Touch Visualization

After commissioning the ZigBee device and mapping it into KNX objects, you can use those KNX objects for creating widgets in Touch visualization.

Click the cross at the top right to close the Hybrid plugin to be able to start Touch configuration.

On the Start page, click . You get to the visualization configurator.

For more information check the controller user guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?