2505_LSS100400_SW_04.0

Device Information

When you click the Device information icon , you will see a list of information about your device:

  • Manufacturer

  • Device type

  • Firmware version

  • Power source

  • Status for receiving telegrams.

  • Input and output ZigBee clusters.

  • Reported attributes of the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?