2505_LSS100400_SW_04.0

List of Parameters

Device

Parameter

Parameter Description

Avatar dimmers

Indicator light level

LED light intensity (%)

Indicator color

The color of the LED light (white/blue)

LED indicator

LED lighting period (On when load is On/Off, Always On/Off)

Minimum level (1...254)

The minimum dimming level setting

Maximum level (1...254)

The maximum dimming level setting

Dimmer mode

Dimming mode setting – Automatic, RC (trailing edge), RL (leading edge), RL-LED.

Merten dimmer

Switch action

Switch function:

  • Light, Light (inverse*)

  • Dimmer, Dimmer (inverse*)

  • Standard shutter**, Standard shutter** (inverse*)

  • Schneider shutter**, Schneider shutter** (inverse*)

  • Scene – two scene numbers (one up, the other down)

LED indicator

LED lighting period (On when load is On/Off, Always On/Off).

On/Toggle level (1...254, 255 = previous value)

Dimmer lighting level after turning on the dimmer.

Start-up level (0...254, 255 = previous value)

Starting lighting level after power outage.

Minimum level (1...254)

Limitation of the bulb function from below - minimum light value.

Maximum level (1...254)

Limitation of the bulb function from above - maximum light value.

Dimmer mode

Dimming mode setting – Automatic, RC (trailing edge), RL (leading edge), RL-LED.

Motion sensor dimmer

Device type switch/dimmer

Device type setting – dimmer or switch.

Occupancy operation mode

Dimmer on and off setting (Manual mode; Auto; Auto on/off, Manual on/off)

Detection timeout (seconds)

Detection duration.

Ambience light threshold (lux)

If light intensity ≥ ambience light threshold, do not switch on.

Rotary dimmer

On/Toggle level (1...254, 255 = previous value)

Dimmer lighting level after turning on the dimmer.

Start-up level (0...254, 255 = previous value)

Starting lighting level after power outage.

Minimum level (1...254)

Limitation of the bulb function from below - minimum light value.

Maximum level (1...254)

Limitation of the bulb function from above - maximum light value.

Dimmer mode

Dimming mode setting – Automatic, RC (trailing edge), RL (leading edge), RL-LED.

Free locate switch

Indicator light level

LED light intensity (%).

Indicator color

The color of the LED light (white/blue).

Key 1 – 4

Button function setting – No configuration/ Toggle dimmer/ Scene.

Switch mode

Setting the number of rockers.

Switch action

Rocker function:

  • Light, Light (inverse*)

  • Dimmer, Dimmer (inverse*)

  • Standard shutter**, Standard shutter** (inverse*)

  • Schneider shutter**, Schneider shutter** (inverse*)

  • Scene – two scene numbers (one up, the other down)

Motion sensor

Sensitivity level

Motion detection sensitivity setting – Default, Low, Medium, High

Detection timeout (seconds)

Detection duration.

Shutter

Switch action

Switch function:

  • Light, Light (inverse*)

  • Dimmer, Dimmer (inverse*)

  • Standard shutter**, Standard shutter** (inverse*)

  • Schneider shutter**, Schneider shutter** (inverse*)

  • Scene – two scene numbers (one up, the other down)

Indicator light level

LED light intensity (%).

Indicator color

The color of the LED light (white/blue).

LED indicator

LED lighting period (On when load is On/Off, Always On/Off).

On/Off transition time

Total movement time of the shutter until fully closed/opened (tenth of a second).

Motor type channel 1/2

Setting the type of motor - asynchronous or pulse motor.

Height: time from fully closed to fully open (seconds)

Time from fully closed to fully open (seconds)

Height: time from fully open to fully closed (seconds)

Time from fully open to fully closed (seconds)

Tilt: time from fully open to fully closed (seconds, 0 = tilt disabled)

Time from fully open to fully closed (seconds, 0 = tilt disabled)

Scene

Number of scene (button press = trigger).

Switch

Indicator light level

LED light intensity (%).

Indicator color

The color of the LED light (white/blue).

LED indicator

LED lighting period (On when load is On/Off, Always On/Off).

Switch action

Switch function:

  • Light, Light (inverse*)

  • Dimmer, Dimmer (inverse*)

  • Standard shutter**, Standard shutter** (inverse*)

  • Schneider shutter**, Schneider shutter** (inverse*)

  • Scene – two scene numbers (one up, the other down)

Motion sensor switch

Occupancy operation mode

Light on and off setting (Manual mode; Auto; Auto on/off, Manual on/off).

Detection timeout (seconds)

Detection duration.

Ambience light threshold (lux)

If light intensity ≥ ambience light threshold, do not switch on.

Inverse* = Reverse order of switches (up/down is down/up) or dimming direction.

Schneider shutter** = Schneider shutter data points are supported.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?