2505_LSS100400_SW_04.0

Device Pairing Mode

To pair the device with the controller, you need to put it in pairing mode.

Press the Reset/Setup button three times briefly until the LED on the front starts blinking orange.

The device is in pairing mode.

NOTE: If your device is flashing green, it is already paired. If you want to pair your device again or to another device, reset it first and repeat the pairing process.

NOTE: For more information on how to pair your wireless device, please refer to its user guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?