2505_LSS100400_SW_04.0

Sockets

Device

Object

Object Description

Sockets

On/Off control (1 bit)

Turn on/off.

On/Off status (1 bit)

Feedback for on/off.

Active power (4 bytes floating point)

Current power consumption.

RMS voltage (4 bytes floating point)

Value of electric voltage.

RMS current (4 bytes floating point)

Electric current.

Energy delivered (4 bytes floating point)

Cumulative energy consumption. The value is reset to zero during commissioning.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?