2505_LSS100400_SW_04.0

Thermostats

Device

Object

Object Description

Thermostat

Battery level (1 byte scale)

Device battery level.

Keypad lockout control (1 byte unsigned / 8 bit enum.)

Disable/Enable keypad functionality.

Temperature (2 bytes floating point)

Temperature detection (°C).

Humidity (1 byte scale)

Humidity detection (%).

Setpoint (10..30°C) – 2 bytes floating point

Required temperature.

Occupied heating setpoint control (2 bytes floating point)

Required temperature for heating mode.

Occupied cooling setpoint control (2 bytes floating point)

Required temperature for cooling mode.

Heating control (1 bit)

Heating mode de/activation.

Cooling control (1 bit)

Cooling mode activation/deactivation.

Remote temperature value (2 bytes floating point)

External sensor temperature.

Local temperature / Temperature (2 bytes floating point)

External sensor temperature or temperature measured by the device.

Occupied heating setpoint status (2 bytes floating point)

Feedback for required temperature for heating mode.

Occupied cooling setpoint status (2 bytes floating point)

Feedback for required temperature for cooling mode.

Heating status (1 bit)

Feedback for heating mode (if active).

Cooling status

Feedback for cooling mode (if active).

Heating demand status (1 byte scale)

Valve position or heating pulse width modulation (in percentage).

Cooling demand status (1 byte scale)

Valve position or cooling pulse width modulation (in percentage).

Fixed Load Demand (4 bytes unsigned integer)

Nominal load power (for power and energy calculation).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?