2505_LSS100400_SW_04.0

Monitor

Monitoring is an information and diagnostic tool that allows you to get an overview of the functionality of the ZigBee network. The Monitor function monitors the activity of the device in the network and the values generated/received by the devices.

To run the monitoring, do the following:

  1. Click > select Monitor.

  2. Click the Start monitor button to start monitoring.

Messages start to appear on the screen in chronological order, containing the following information about the devices:

Number: Message serial number.

Time: The time when the message was received by the hybrid module.

Type: Data sent/received (S/R) and signal strength.

Address: MAC address of the device.

Cluster: Type of the ZigBee clusters.

Action: Action taken (related to the cluster).

Data: Data sent/received.


If you want to stop monitoring, click Stop monitor.

You can export monitoring values as a CSV file to local storage: click Export CSV.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?