2505_LSS100400_SW_04.0

Free Locate Switch

Device

Object

Object Description

Free locate switch

Battery level (1 byte scale)

Device battery level.

 

On/Off/Toggle (1 bit)

On/Off/Toggle control.

 

Start/stop dimming (4 bits)

Button press dims 100 percent up or down. Releasing the button stops dimming.

 

Set level or step current value (1 byte unsigned)

Dimming by a set step.

 

Step size (0 = default)

Setting the dimming step range.

 

Scene (1 byte unsigned)

Sends number of the scene.

Merten

Up/Down/Stop (4 bits)

Button press dims 100 percent up or down. Releasing the button stops dimming.

 

Up/Down (1 bit)

1 = dimming up, 0 = dimming down

 

Stop (1 bit)

0 = stop dimming

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?