2505_LSS100400_SW_04.0

Delete ZigBee Devices

The last red icon in the device line is for removing ZigBee devices from the network.

If you want to delete your device, click at the end of the device line > click Yes.


The device will be removed from the network.

Reset the device physically so that it can join the network again.

You have to reset battery-powered devices manually to fully remove them from the network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?