2505_LSS100400_SW_04.0

Extend Device Functionality

Mains-powered ZigBee devices with manual control (push-buttons, rotary knobs) have extended functionality of decoupling the front and back of the device. The front (push-buttons) part of the device can control a completely different device than the one it belongs to.

A blue note in the device Configuration dialog informs you of the extension possibility.

Devices without a push-button interface, like the Wiser micro-modules, do not support this extended functionality.


To use this functionality, do the following:

  1. Go to Hybrid plugin > select a device that supports this functionality > click to open its Parameters setting.

  2. In device Parameters setting, select from a drop-down menu which device type you want to control by switch action.

  3. Click Save.

  4. Click to open the Configuration dialog > configure your device.
    There are three sections in the Configuration dialog:

    • Name and device location.

    • Configuration of the back part of your device (device control, device status).

    • Push-button configuration (if your device supports it) at the front panel (buttons, knobs).



  5. In the Push-button section, based on the setting you did in the Parameters section, you can see the functionality assigned to the front part of the device.
    Assign a group address to each functionality.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?