2505_LSS100400_SW_04.0

Logs

The network log is a direct access data set that stores messages and commands, communications about network functions.

You can gather every packet or a set of packets for further analysis, traffic monitoring, or troubleshooting.

To see the logs, click > Logs:

Several kinds of information can appear in your network log:

  • Job time, step time, and data entered by user-written routines.

  • Operating data.

  • Descriptions of unusual events.

You can reload logs (click Reload logs) and export them in a *.txt file to your local storage (click Export logs).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?