2505_LSS100400_SW_04.0

Getting Started

You need a Wiser for KNX or spaceLYnk controller to operate the Hybrid Module.

Before you install the Hybrid plugin into the Wiser for KNX or spaceLYnk controller, make sure your Hybrid Module is:

  • POWERED: The device is powered by 24 V DC.

  • PROPERLY WIRED TO THE CONTROLLER: You have to cross the RX and TX wires, as shown in the diagram.

    You can find detailed information on the wiring in the installation instructions of the Hybrid Module.

You need a standard web browser to work with the configuration software of the logic controllers, plugin and to set up the Hybrid Module.

Recommended browsers:

  • Chrome version 118.0.5993.89 (Official Build) 64-bit

  • Firefox version 118.0.2 (64-bit)

  • Safari version 15.6.1

Make sure your logic controller has a firmware version of at least 2.8.3 (or higher).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?