Device Firmware Upgrade
By default, automatic device firmware update is disabled. With the Firmware upgrade icon you can manually upgrade the device firmware.
There is no new firmware available for
the device.
If new firmware is available for the device (the
device is colored blue), you can start the firmware upgrade:
Click > Yes > If you want to upgrade a battery device, interact
with it to wake it up > click Continue.
The device will turn green (Firmware upgrade in progress) and then white (Configured and operational). Firmware upgrade is completed.
If you do not want to upgrade your device firmware
manually, enable automatic firmware upgrade of your device as follows:
Click > check Enable automatic firmware
upgrade.
Your device firmware will be automatically upgraded whenever a
firmware update is available. You can find information about the firmware
version of your device if you click next to your device (Device Information).