Archive Services Configuration
Once you have configured the Archive Services configuration file (ArchiveServices.exe.config), you must start Archive Services in order to run Responder Archive Explorer. You may enable multiple Archive Services to enhance Archive Explorer performance.
The Count field indicates the number of Archive Services running. If you change this value to 0 and click Apply, the Arguments field becomes enabled. Use this field to set your geodatabase server along with any arguments.
To start Archive Services, enter the number of instances you'd like to run in the Count field and click Apply. When Archive Services are running, you may not edit the Arguments field. The Path field always remains disabled. This field provides the path to the executable that launches Archive Services.
Arguments
Below is a list of available arguments.
|
Argument |
Description |
|---|---|
|
-fast |
Does not initialize the geometric network on start-up. |