Responder Line Display
The RxLineDisplay class must have permissions that allow users to write data to it.
-
Login to the geodatabase using the same login user entered for the geodatabase in the Data Services configuration file (Look for <user> and <password> in the first block of code on the Data Services Configuration page).
-
New Implementation: Create a non-versioned feature class with a type of Line Features. You can name this feature class anyway you'd like. In this example, we'll call it RxLineDisplay. Because it's non-versioned, this feature class cannot be created within a versioned data set. Create it outside of a data set or within a non-versioned data set.
Upgrade: The RxLineDisplay feature class may already exist. Make changes based on the instructions below.
IMPORTANT: The RxLineDisplay feature class must use the same coordinates system as the Electric dataset. If it does not, you will experience errors. The error may look something like this one: System.Runtime.InteropServices.COMException (0x80040215): Exception from HRESULT: 0x80040215 at Esri.ArcGIS.Geometry.PolylineClass.Union(IGeometry other) -
New Implementation: When you are prompted to add fields, add the following fields. You may add more, but those listed below are required. You may name them any way you'd like.
-
RxFeederID: Text data type
-
RxPhase: Text data type
-
RxFCID: Long Integer data type (Optional: To display the Feature Class name instead of the FCID add a domain and assign it to this field.)
-
RxOID: Long Integer data type
-
RxSUBID: Long Integer data type
-
RxX: Double data type
-
RxY: Double data type
-
CONDUCTORFCID: Long Integer data type (Optional: To display the Feature Class name instead of the FCID add a domain and assign it to this field.)
Upgrade: Ensure the fields above are added and delete the following fields, if they exist in the feature class:
-
RxIncidentId: Long integer data type
-
RxDeviceId: Long integer data type
NOTE: If you are upgrading Responder, you will need to add the RXLINEDISPLAY model name to the Responder Object Class Model Names domain. Add the RXFEEDERID, RXPHASE, RXRESPONSIBLEDEVICEFCID, RXRESPONSIBLEDEVICEOID, RXRESPONSIBLEDEVICESUBID, RXRESPONSIBLEDEVICEX, RXRESPONSIBLEDEVICEY, and RXCONDUCTORFCID model names to the Responder Field Model Name domain. If you are implementing Responder for the first time, these model names were added in a previous step. -
-
Use the ArcFM Properties Manager to assign the RXLINEDISPLAY model name to the RxLineDisplay feature class you just created. Assign the following field model names on this class (model names in all caps):
-
RxFeederID: RXFEEDERID
-
RxPhase: RXPHASE
-
RxFCID: RXRESPONSIBLEDEVICEFCID
-
RxOID: RXRESPONSIBLEDEVICEOID
-
RxSUBID: RXRESPONSIBLEDEVICESUBID
-
RxX: RXRESPONSIBLEDEVICEX
-
RxY: RXRESPONSIBLEDEVICEY
-
CONDUCTORFCID: RXCONDUCTORFCID
-
-
Click OK to close the ArcFM Properties Manager and save changes.
-
From Windows Services, reset Data Services.
By default, this functionality is turned off in the Data Services configuration file. Before Responder Line Display can be symbolized in the map, you must follow the steps below to enable the functionality.
-
Open Miner.Responder.DataServices.exe.config. By default, this file is installed in: \Program Files (x86)\Miner and Miner\Responder\Server\.
-
Look for the following bit of XML:
<add key="ResponderLineDisplay" value="false" />
-
Change the value to True.
NOTE: Upgrade: If you have already enabled Line Display, this is automatically set to True. -
Save and close Miner.Responder.DataServices.exe.config.
-
To view Responder Line Display on the map, add the RxLineDisplay layer to your Responder_Cached group in ArcMap. You can modify the symbology on the Display tab.
Optional: There is an optional class level model name to exclude specified conductor/line feature classes from having any line display drawn. To use this functionality, add RXEXCLUDEFROMLINEDISPLAY to the Responder Object Class model name domain. Then, assign this model name to any conductor/line feature class to exclude them from Line Display. Feature classes excluded from Line Display will not store or display Line Display information for future use.
Please note that ArcMap allows you to change the stored display per feature class to set the view at any scale. So, to include the Line Display when zoomed in, but not at a higher elevation, change the stored display.
You can update the stored display to show STATUS and symbolize the 0, 1, and 3 values. An example of possible values include:
0 - Line Display in Awaiting Processing
1 - Line Display in Process
3 - Line Display is Finished Processing (This will be the status most often displayed.)
Optional: You can configure the Responder Phase Swap line display label that appears in ArcMap through the Miner.Responder.LineDisplayService.config file. By default, this file is installed in: \Program Files (x86)\Miner and Miner\Responder\Server\.
-
In the config file, locate <add key="LineDisplayPhaseSwapString" value="{0} To {1}" />
-
You can change the value to represent phase swap as desired. Use {0} to represent the energized line doing the phase swap, and {1} as the de-energized line. Here are some examples:
-
value="Energizing from {0} to {1}"
-
value="{1} Receiving from {0}"
-
value="Phase swap on {1} from the Energized {0} line"
-
-
Save and close the config file. You may need to restart services for this change to take effect.
Symbology
You can determine how Responder Line Displays appear on the map. This section discusses an example of how you might set up this symbology. Responder recognizes four types of lines: normal state, de-energized, differently energized, and Responder phase swap. De-energized means the line is getting no electricity and the RxFeederID field will always be Null to indicate this. Differently energized means the line is being fed in some way that's not usual (e.g., backfed or multifed). Responder Phase Swap indicates the line is being backfed with a different phase than the phase on the line. The RxFeederID field will contain the value of the feeder providing electricity to the line. You can create separate layers in ArcMap to display the Responder Line Display symbology for each of these types of lines.