RX_GLOBALID_XREF

This table is used only when you have implemented the optional Esri replication support. In order to support Esri replication, Responder requires this table to help manage GUIDs.

Field Name

Description

FCID

The feature class ID of the feature impacted by an incident.

OID

The object ID of the feature impacted by an incident.

GLOBALID

The GlobalID (GUID) of the feature impacted by an incident.

FCID_ACTUAL

Currently not used by Responder. This field should contain the FCID of the feature as it appears in the replicated database.

OID_ACTUAL

Currently not used by Responder. This field should contain the OID of the feature as it appears in the replicated database.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?