RX_INC_DEV_ASSIGN_HISTORY

Field Name

Description

INC_DEV_ASSIGN_ID

The ID of the device assignment. This field serves as a foreign key to the RX_INC_DEV_ASSIGNMENTS table.

INCIDENT_DEVICE_ID

The ID of the incident device. This field serves as a foreign key to the RX_INCIDENT_DEVICES table.

CREW_ASSIGNMENT_ID

The unique identifier assigned to each crew assignment. This field corresponds with the ID field in the RX_CREW_ASSIGNMENTS table.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

CHANGE_DATE

The date an operation was performed on the incident device.

OPERATION

The operation (e.g., insert, delete, update) performed on the incident device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?