RX_INC_DEV_ASSIGN_ARCHIVE
Field Name |
Description |
---|---|
INC_DEVICE_ASSIGN_ID |
ID from the incident device assignment table. Corresponds to the ID field in the RX_INC_DEV_ASSIGNMENTS table. |
INCIDENT_DEVICE_ID |
The unique identifier assigned to the incident device. This field corresponds to the ID field in the RX_INCIDENT_DEVICES table. |
CREW_ASSIGNMENT_ID |
The unique identifier assigned to each crew assignment. This field corresponds with the ID field in the RX_CREW_ASSIGNMENTS table. |
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
CHANGE_DATE |
The time and date an operation was performed on the record. |
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
INCIDENT_ID |
The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table. |