Prediction Services Console

Use the console to manage your existing instances of Prediction Services. By default, the Configuration screen is displayed. Click the link to Console to manage your Prediction Services or Prediction Mode to enable prediction or set the appropriate mode.

If you are running multiple instances of Prediction Services, there will be multiple console windows (one for each instance). To use a command, enter it in the Input field and click Send. The results of the command are displayed in the windows for each Prediction Services instance running. The various commands you can use in this window are listed in Responder Services Commands.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?