RX_SWITCHING_ORDER_FEATURES

Field Name

Description

OID

Object ID of the feature that was operated upon.

FCID

Feature class ID of the feature that was operated upon.

SUBID

The unique ID of each segment of a complex edge.

X

The x-coordinate of the incident device.

Y

The y-coordinate of the incident device.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

FACILITY_ID

The Facility ID of the incident device as defined in the geodatabase.

REGION

The region in which the switching order feature is located. This field uses the REGION domain.

SUBSTATION

The substation that feeds the device.

COMMENTS

Notes from the operator or dispatcher.

ENABLED

Not used.

SUBTYPE

The subtype of the device.

FEEDER_ID

The ID of the feeder.

PHASE_DESIGNATION

The phase designation of the device.

OPERATING_VOLTAGE

The operating voltage of the device.

NAME

The name assigned to the device.

SW_ORDER_REQUEST_ID

The unique ID assigned to the switching order request.

AFFECTS_ENERGIZATION

Indicates whether the feature participates in the geometric network (electric device) or not (location feature).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?