TmScenarios Table
Field |
Description |
---|---|
Scenario |
A unique number identifying the scenario. This field is a primary key. |
Name |
A description for the scenario. |
Device Facility ID |
The Facility ID of the outage device. |
Device Type |
The Type of the outage device. |
DeviceFcid |
Feature class ID for the incident device. |
DeviceOid |
Object ID for the incident device. |
Customers Affected |
The number of customers affected by the outage. |
NumberCalls |
The number of customers that called in the scenario. |
NumberHazards |
The number of hazards in the scenario. |
Comments |
Comments about the outage. |