Modify Scheduled Switching Order Filter
The Scheduled Switching Orders window in Responder Explorer provides a filter that allows you to limit the number of switching orders displayed. If you select All Scheduled in the pull-down menu, it will display all past scheduled switching orders that have not been executed as well as all scheduled switching orders eight days in the future. You can modify the number of days (or hours/minutes) in the future scheduled switching orders are displayed. To do this, modify the Miner.Responder.Explorer.exe.config file.
- On the client machine, browse to and open Miner.Responder.Explorer.exe.config. By default, this file is installed here: C:\Program Files (x86)\Miner and Miner\Responder\Client.
-
Locate the following XML.
<add key="SwitchOrdersSchedule.MaxTimeWindow" value="8"/>
- Set the value to the maximum timeframe to display scheduled switching orders. For example, to display all scheduled switching orders two weeks out, set the value to 14. This attribute takes a value of d.hh:mm:ss.
- Save and close Miner.Responder.Explorer.exe.config.